Selecciona tu región e idioma

Menú

General information:

Hitachi Energy is seeking for a Field Supervisor and Tester for it's Earth City, MO location.Transformer Service Supervisors have the detailed knowledge to perform installation, repair, and service of power transformers and Testers have the technical knowledge and ability to perform standard electrical testing. Work is performed on customer sites and requires extensive travel.

Responsibilities:

Leading and working alongside crews ranging from 2 to 8+ technicians to complete assigned projects. Projects may include but are not limited to the installation, repair, testing, maintenance, relocation, scrap, inspection, and retrofit of transformers with high-side voltages ranging from 4160V to 765kV. Act as the onsite point of contact for the customer and subcontractors during project execution. Strategically assign tasks to crew members in order to minimize cost and project duration considering crew skillsets, site conditions, weather forecasts, etc. Proactively identify and report project nonconformances to Project Management and Engineering for timely resolution Perform electrical testing of transformers and reactors including but not limited to bushing power factor & capacitance, core megger, CT ratio & polarity, TTR, winding resistance, insulation power factor, insulation resistance, excitation, SFRA, DFR, leakage reactance, and control cabinet functional checks. Provide input and expertise during the project-planning phase regarding project schedule and manpower requirements. Practice and promote a safety-first approach; always maintain compliance with all Hitachi Energy and customer EHS requirements. Living Hitachi Energy's core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Your background:

High School Diploma/GED and minimum 5 years of professional work experience, or Associate Degree and minimum 3 years of professional work experience. Candidate must already have work authorization that would permit them to work for Hitachi Energy in the United States. Thorough knowledge of transformer field service operations and transformer field testing. Knowledgeable and fully fluent in transformer installation and assembly, vacuum and oil processing, shell and/or core form transformer designs, and components internal to the transformer. Proficiency with Load Tap Changer (LTC) maintenance and repair is a plus. Experience welding above and below oil on transformer tanks is a plus. Possession of a Class A CDL is a plus. Must have a valid driver's license and ability to travel up to 85%.

Ubicación Remote - Missouri, United States of America
Tipo de empleo Full time
Experiencia Experienced
Función laboral Engineering & Science
Contrato Regular
Fecha de publicación 2023-07-18
Número de referencia R0027719

Sobre Hitachi Energy

Hitachi Energy es un líder tecnológico mundial que promueve un futuro energético sostenible para todos. Prestamos servicio a clientes de los sectores de servicios públicos, industria e infraestructuras con soluciones y servicios innovadores en toda la cadena de valor. Junto con nuestros clientes y socios, somos pioneros en tecnologías y facilitamos la transformación digital necesaria para acelerar la transición energética hacia un futuro neutro en carbono. Estamos haciendo avanzar el sistema energético mundial para que sea más sostenible, flexible y seguro, equilibrando al mismo tiempo el valor social, medioambiental y económico. Hitachi Energy tiene un historial probado y una base instalada sin precedentes en más de 140 países. Con sede en Suiza, empleamos a unas 45.000 personas en 90 países y generamos volúmenes de negocio de unos 13.000 millones de dólares.

www.hitachienergy.com

Hitachi Energy es una empresa que promueve la Igualdad de Oportunidades en el Empleo (Equal Employment Opportunity)(EEO) y la Acción Afirmativa, fomentando la diversidad en el lugar de trabajo. Los invitamos a presentar su candidatura y queremos que sepa que todos los solicitantes cualificados serán tenidos en cuenta para el empleo independientemente de su raza, credo, color, ascendencia, religión, sexo, origen nacional, condición de ciudadano, edad, orientación sexual, identidad de género, discapacidad, estado civil, situación de baja médica familiar, condición de veterano protegido o cualquier otra característica legalmente protegida. Para obtener más información sobre sus derechos como solicitante de empleo, visite los siguientes sitios web aquí y aquí. Los veteranos protegidos y las personas cualificadas con una discapacidad pueden solicitar una adaptación razonable si no pueden o tienen limitada su capacidad para utilizar o acceder al sitio profesional de Hitachi Energy como consecuencia de su discapacidad. Puede solicitar ajustes razonables llamando a un representante de Recursos Humanos de Hitachi Energy al 1-888-504-2007 o enviando un correo electrónico a: [email protected]. No se aceptarán currículos ni solicitudes de esta manera.