Choose your region and language

Go

Menu

DRIVE TOWARD AN ELECTRIC FUTURE

Let’s connect, charge & optimize.

Are you preparing to scale up your electric vehicles? If so, then charging infrastructure upgrades are next. Charging locations will need smart charging solutions with minimal footprint, stationary battery energy storage solutions to offset peek demands on the grid, and an energy management system to optimize operations at the lowest cost. Whether for private, public or commercial needs, Hitachi Energy has solutions to help you conquer the energy transition and get your infrastructure up to speed.

Connect

to the grid with the help of unparalleled grid expertise​

Charge

your e-fleets with our space efficient hardware solutions​

Optimize

operations & maintenance with digital solutions
Market: Transportation
GET ON BOARD

Your needs are EV-olving.

Electric fleets come in all different shapes and sizes. The heavier the load, the more power is needed. Our solutions are designed to optimize your existing infrastructure and help you scale up quickly while maintaining operations. ​

Hitachi Energy offers a compact, sustainable, scalable, reliable end-to-end solution from the grid to the plug which ensures ongoing operational excellence. We help you build an integrated & open ecosystem which includes advanced energy management that will offer visibility and actionable insight from the field to boardroom at the lowest operational costs.​

>> The heavier the load, the more power you need. >>

Aerial view of parking lot for car sharing business. Electric cars charging at charging station and powered by solar panel. 3D rendering image.

Charging station & hubs​

For low power on-the-go needs​

Public transport​

For depots and Electric Bus Rapid Transit (EBRT)​
Electric truck and van charging at charging station powered by solar panel system. 3D rendering image.

Commercial & Logistic​

For megawatt power at depots and en route​

Offroad & special vehicles​

For high power static & dynamic charging​

KEEP FLEETS MOVING

Check out our Land solutions

Looking to design, build, operate or maintain assets? Hitachi Energy is a full lifecycle trusted partner - from planning, to design, operation & maintenance. Your transformation journey towards smarter mobility starts here with our ​land transportation electrification.

Hardware​

Hitachi Energy Logo

Semiconductors

Hitachi Energy’s advanced semiconductor technology has created almost unlimited control possibilities in energy transmission systems. We lie at the heart of traction converters driving high-speed trains, metros, and diesel-electric locomotives. And the many pumps, fans, roller tables, hoists, and winches found throughout the industry rely on us. Today we are also powering the next generation of e-vehicles enabling people to enjoy greener mobility.

Power electronics play an important role in electric mobility, as they handle the efficient power transmission from the battery to the motor. As a new semiconductor base material, silicon carbide offers lower conduction losses and higher switching frequencies. It is essential for the system that the interfaces and internal structure of the power electronics are optimized for low stray inductances for maximum pay-off.

The performance of a switch or an inverter for xEV vehicles can be increased with an optimized design of the load current paths. This means that the advantages of SiC can be fully utilized for greater efficiency, either resulting in a greater range or a more compact design for the electric drivetrain.

Hitachi Energy’s SiC e-mobility module, RoadPak, pushes the boundaries of power density and reduces stray inductance to new levels.

Typical applications are:

  • Cars: Scalable current and power ratings support inverter platforms of various e-cars
  • Trucks: High power in a small package allows efficient inverter design of e-trucks
  • Public transport: High reliability for the typical stop-and-go operation of e-buses and trams
  • Aviation: Performance and reliability to meet the demands of a wide range of aviation applications
  • Charging: Delivers performance to enable fast charging of e-trucks and e-buses
FEATURED CONTENT

Hitachi Energy is on a mission to decarbonize EV fleets around the globe. Learn about how you can transform your business to meet your business’ sustainability goals.

Turning challenges into opportunities for transportation fleet electrification IDC Spotlight

Turning challenges into opportunities for transportation fleet electrification

Webinar 17-03-2022 - 17-03-2022 Online

Powering the future of public transport

Powering the future of public transport. Charging strategies for bus fleets
Part of categoryBlog Post
30-05-2023 | 4 min read

Accelerating the electrification of public transportation at UITP

The time to connect, charge and optimize your e-fleets is now. Get ready to move with us.

Blogs & News

CUSTOMER SUCCESS STORIES

See our solutions in action

For over 100 years, Hitachi Energy has partnered with transportation customers around the world on transformation projects that help them meet their sustainability goals.

Let's Connect

We're eager to partner with you!

GO THE EXTRA MILE

Ready to transform your fleet?

Today’s demands on fleet operators are rising. Whether in commercial & logistic, public transport, offroad & special vehicles or charging hubs, all fleets will evolve.​

Connect, charge and optimize your fleets with Hitachi Energy.​

Let’s get to work! ​