About the customer
Silicon Valley Power (SVP) is a municipal utility that provides electricity to 52,000 customers across 19.3 square miles in city of Santa Clara, California, the heart of Silicon Valley. Eighty-four percent are residential customers who consume 8.7% of power sales while 1,839 industrial customers comprise 88% of the utility’s power sales. Industrial customers include large Fortune 500 companies such as Applied Materials, Microsoft, National Semiconductor, NVIDIA, Owens Corning, Oracle, and Yahoo.
SVP owns, operates and participates in 800 megawatts of electric generating resources (at least 25% of which is from renewable power sources) and serves a peak load of approximately 470 MW. SVP also owns and operates a 60-mile, four-ring 144 and 288 Mbps fiber backbone that connects SCADA and 28 substations, 37 data centers (dark fiber leasing program), 27 public schools, as well as local fire stations, libraries, and many other city government facilities.
The Evolution of SVP’s Smart Grid Plans
In 2012, the utility achieved 99.994% system wide availability to customers. That same year, SVP was ranked first in the nation for business customer satisfaction based upon an annual survey conducted by E Source Business Marketing Services. Customers cited the utility’s reliable power service and efforts to keep prices low as the primary reasons for the positive rating.
Before AMI
SVP’s power utility infrastructure includes 28 substations, 10,000 utility power poles and 8,000 street light poles which are owned and maintained by the City. There are 52,000 electric meters and, like many utilities, most commercial and residential meter reading was done manually on a monthly basis. The same meter readers also had responsibility for manually reading 27,000 municipal water meters. Meter readers in the field were equipped with a handheld unit that was used for input of meter readings and was capable of automatically reading the approximately 8,300 residential power meters enabled with walk-by radio interrogation for consumption data. At the end of the day, the handheld devices were placed in a cradle at SVP offices to upload the meter data for analysis and billing.
SVP connected to its largest industrial customers over dial-up lines using Itron MV-90 Data Collectors which enabled periodic polling of data collected and stored at the customer site. Direct customer connectivity was also used to enable and verify SVP’s ”Power Reduction Pool” program, a voluntary load-shedding program that was created ahead of the energy crisis to avoid the need for rolling blackouts in Santa Clara. During system emergencies, SVP customers collectively reduce power by as much as 10 MW within 30 minutes. As a result, customers in Santa Clara did not see a single rolling blackout during the crisis.
SVP MeterConnect™ Conceived
In 1990, SVP began exploring advanced meter reading requirements, technologies, and benefits.
Key benefits identified which would contribute to customer satisfaction included:
- increased distribution system reliability
- reduced time to detect and pinpoint outage locations
- ability to improve service and maintain lower cost of power to customers
- increased meter reading accuracy
- more timely access to metering data (especially critical in system planning for industrial customers) −−faster customer response time with ability to perform remote on/off service
- reduced operational costs
As SVP started considering the range of utility applications which comprise a smart grid, they realized a narrowband network could not provide enough bandwidth and performance to meet future needs, however, a wireless broadband network could. They developed the vision of a single citywide wireless network that could be used for AMI, distribution automation, outage detection, mobile workforce (work orders, trouble tickets, GIS, reports, etc.), disaster communications, and more. SVP proactively explored interest in a citywide wireless broadband network and quickly came to the conclusion that there was significant interest from other city departments – police, fire, water, transportation, building and fire inspectors, and recreation departments – all of whom had interest which would make this approach cost effective. Up until this time, those city departments that had networks utilized proprietary systems that did not cross departments and were not centrally managed thereby increasing operational costs. The events of 9/11 further strengthened the city’s resolve that a common wireless broadband network for municipal services was the right approach for them to take to ensure all city workers could easily communicate and collaborate to better service the community.