Choose your region and language

Go

Menu

TrafoSiteRepair™

Our on-site repair is achieved by bringing the transformer factory setup to the work site. TrafoSiteRepair™ service is executed to the same high-quality standard as a workshop repair. This is done by mobilizing special equipment and tools needed to perform any scope of work, from refurbishment and upgrades to replacing all windings manufactured in transformer factories under strict quality standards.

TrafoSiteRepair™ has been used worldwide for the repair of over 400 transformers, including ultra-high-voltage and converter transformers, industrial units, and shunt reactors. TrafoSiteRepair™ has saved utilities and industrial users millions of dollars by reducing downtime in installations where production losses per day can be extremely high. With on-site repair, transport to a repair facility can be avoided, reducing risk and saving cost and time.

Significant progress in power electronics led Hitachi Energy to develop TrafoSiteTesting™, a compact high-voltage test system, and Low-Frequency Heating, a special Hitachi Energy technology for high-temperature transformer drying out in the field. TrafoSiteTesting™ enables on-site high-voltage laboratory testing such as applied and induced voltage tests with partial discharge measurements, heat run, and impulse tests.

TrafoSiteTesting™ may also be used for condition assessment (preventive measure), transformer troubleshooting (failure identification and localization), and as an extra quality check measure on new units after transportation and installation.

Low-frequency heating technology decreases the drying time by more than 50% compared to conventional methods and is capable of reducing moisture in cellulose to less than 1%.

Hitachi Energy's TrafoSiteRepair™ provides customers with a complete transformer on-site solution by combining state-of-the-art technology with our extensive experience.

Product image for: TrafoSiteRepair™
On-site Repairs
Hitachi Energy offers on-site repairs to bring the transformer factory setup to the work site with the TrafoSiteRepair™ service that is executed to the same high-quality standard as a workshop repair.
Upgrade, Repair, & Extend
Hitachi Energy offers customized solutions to extend the life of your transformers.
Parts & Maintain
Hitachi Energy offers genuine, high-quality spare parts along with basic and advanced maintenance services.

Our Global Service Teams are here to support you anytime!

Get to know more

Transformer service
Aging assets, rising energy demand, and the critical need to avoid unplanned outages are challenging worldwide utilities and industrials. The service portfolio of Hitachi Energy allows utilities and industrials to maximize the return on transformer assets by ensuring high reliability, reducing life cycle costs, and ensuring optimized performance while lowering environmental impact.
Transformers
Hitachi Energy offers distribution and power transformers, Dry-type and EconiQ™ Transformers as well as services, for industrial and commercial applications.
Transformer Insulation and Components
The world's broadest and most reliable portfolio of transformers components and insulation