Choose your region and language

Go

Menu

Oil Regeneration or Reclamation

Oil ages during the operating life of a transformer. By performing oil reclamation, where the oil is passed through an absorbent, the oil can be reinserted into the transformer in a new state.

Oil is a natural material that ages due to the operating environment and transformer properties. Through oil sampling and analysis, the condition of the oil can be inferred. Aged oil demonstrates a higher concentration of oxidation and acids.

Oil reclamation or oil regeneration is a process whereby oil is processed to achieve a significant condition improvement, aimed at being as close to “as new” as possible, by removing the aging products. The processing is performed while a transformer is in service to achieve maximum effectiveness with minimum impact on on-site operations. The oil affects the insulation in the transformer, and the insulation affects the oil; hence the condition of the oil impacts the expected life of the transformer.

The modern reclaiming technology with the reactivation of the absorbent makes it economically feasible to use much more active absorbent material. Typically 5-10 times more absorbent is used compared with the old conventional systems. This leads to a much better cleaning effect on the paper and to the excellent long-term stability of the reclaimed oil.

For some transformers, there is data available for up to 10 years after reclamation. The data shows very little change in acidity and color after 10 years of operation since the oil was reclaimed.

To prevent excessive production of acids due to oil degradation, it is recommended that the oil be reclaimed before it is severely degraded. Low molecular weight acids migrate into the paper insulation and become much harder to remove than from the oil.

The essential elements of the online reclamation technology are that the absorbent is automatically reactivated after each cycle and that the transformer remains in operation. The reactivation allows for using much more active absorbent than with the classical type of reclaiming plants, where the Fullers' earth needs to be replaced frequently and thereafter disposed of. The final step is to restore the inhibitor content.

Oil Regeneration-Advanced Maintenance for Transformers Service

Scope of work

The essential elements of the online reclamation technology are that the absorbent is automatically reactivated after each cycle and that the transformer remains in operation. The reactivation allows for using much more active absorbent than with the classical type of reclaiming plants, where the Fullers' earth needs to be replaced frequently and thereafter disposed of. The complete oil volume is typically circulated 8 to 12 times over the Fullers' earth to achieve a long-lasting effect. The final step is to restore the inhibitor content.

The modern reclaiming technology with the reactivation of the absorbent makes it economically feasible to use much more active absorbent material. Typically 5-10 times more absorbent is used compared with the old conventional systems. This leads to a much better cleaning effect on the paper and to the excellent long-term stability of the reclaimed oil.

On-site low frequency heating (LFH) drying

Hitachi Energy offers a plant and process concept that underlines the importance of assessing the insulation system's moisture and temperature. Temperature and vacuum are the main factors for drying speed and drying quality.

Advanced Maintenance

Hitachi Energy provides advanced maintenance services for transformers to be performed on-site that aim to extend the life of your assets.

Parts & Maintain

Hitachi Energy offers genuine, high-quality spare parts along with basic and advanced maintenance services.

24/7/365

Our Global Service Teams are here to support you anytime!

Get to know more

Transformer service

Aging assets, rising energy demand, and the critical need to avoid unplanned outages are challenging worldwide utilities and industrials. The service portfolio of Hitachi Energy allows utilities and industrials to maximize the return on transformer assets by ensuring high reliability, reducing life cycle costs, and ensuring optimized performance while lowering environmental impact.
Hitachi Energy Power Transformers

Transformers

Hitachi Energy offers distribution and power transformers, Dry-type and EconiQ™ Transformers as well as services, for industrial and commercial applications.