选择您的地区和语言

菜单

Hitachi Energy leads the charge with new SF₆-free EconiQ™ solutions

By Dr. Markus Heimbach and Dr. Christian Ohler
22-08-2024 | 6 min read

CIGRE special part 2: Hitachi Energy unveils two iconic SF₆-free world-firsts!

These remarkable SF₆-free solutions underscore the reliability and scalability of our technology.

Welcome to the Power Pulse podcast blog series, where we delve into the exciting world of energy.

The Power Pulse podcast's brand-new season features the brightest minds in the industry as they examine the challenges, opportunities, innovations, breakthroughs, and sometimes serendipities that have played a part in advancing the development of the power grid. Hear them demystify the fascinating workings behind one of the most impressive engineering feats of the modern era - the electricity grid. Plug in! We promise an electrifying experience with every new episode.

Hitachi Energy leads the charge with new SF6-free EconiQ solutions

The call for a new SF6-free world

The power industry is at a crossroads. The growing demand for energy, relentless pursuit of clean energy, and the growing urgency to combat climate change have necessitated a radical overhaul of traditional power systems. A key challenge lies in the widespread use of sulfur hexafluoride (SF6) in high-voltage equipment. While an exceptional insulator and arc quencher, SF6 is a potent greenhouse gas with a global warming potential thousands of times greater than carbon dioxide (CO2).

The CIGRE conference, a biennial gathering of the power system community, has emerged as a pivotal platform for addressing the challenges of decarbonization and energy transition. This year’s event promises to be particularly groundbreaking, as Hitachi Energy unveils its latest advancements in SF6-free technology. The company’s commitment to innovation is evident in its development of the EconiQ gas circuit-breaker and switchgear technology, a revolutionary alternative to SF6–based solutions, that offers exceptional performance without compromising environmental sustainability.

EconiQ milestones unveiled at CIGRE

CIGRE part 2 blog_EconiQ milestones-2

This blog delves into the challenges and opportunities presented by the urgency of accelerated energy transition, exploring the latest advancements in SF6-free technology, and the path toward a more sustainable grid. Tune in to this special episode of the Power Pulse podcast to find out more about this topic. 

We hope you can join us in beautiful Paris as we continue to accelerate the energy transition and create a sustainable energy future for all. Book a meeting with us.

Designing eco-efficient high-voltage products: a life cycle approach

Designing high-voltage products that are both efficient and sustainable involves several key stages:

  1. Vision and planning: Developing a scalable portfolio from 100 kV to 1000 kV, ensuring that the technology can be adapted for various voltage levels and diverse grid requirements.
  2. Innovation in insulation: Utilizing a mixture of carbon dioxide (CO2) and oxygen (O2) with the addition of C4-fluoronitrile (C4-FN) in certain products to maintain compact dimensions without compromising performance.
  3. Testing and validation: Rigorous testing to ensure reliability and safety, comparable to or exceeding traditional SF6 equipment.
  4. Life cycle assessment (LCA): Considering the total carbon footprint of the product, from raw material extraction to final disposal, ensuring minimal environmental impact.
  5. Market introduction: Gradually introducing products, starting with pilot projects, and scaling up based on market acceptance and evolving regulatory frameworks.

The EconiQ portfolio is sustainability-oriented in design to deliver a superior environmental performance compared to conventional solutions.

The regulatory landscape: Global shift away from SF6

Global regulations are increasingly targeting the reduction of SF6 due to its environmental impact. Legislation varies by region, but includes:

  • Technical specifications: Ensuring that products meet stringent safety and performance standards and grids remain as reliable as they currently are.

  • Environmental impact: Minimizing the use of SF6, with exemptions for certain applications where alternatives are not yet viable or where technical performance would be compromised. 

  • Life cycle considerations: Assessing the overall carbon footprint of products, encouraging the development of solutions that offer substantial reductions in greenhouse gas emissions.

Innovating for a sustainable grid: Alternatives to SF6

Several technologies are being explored to replace SF6 in high-voltage equipment. These include various gas mixtures such as the EconiQ gas mixture, vacuum, and air insulation. Each technology has its strengths and limitations. 

replacing-sf6-in-hv_1
  1. Gas mixtures: Using combinations of CO2, O2 and C4-FN to achieve the desired insulation properties and providing the same compactness as SF6 while reducing environmental impact.  
  2. Vacuum interruption: Effective in medium voltage applications, vacuum technology is difficult to scale to higher voltages due to its insulation limitations. 
  3. Technical air: Used in combination with other technologies, technical air can be effective, but requires larger spaces and higher pressures, making it less suitable for compact designs. 

Among these, Hitachi Energy’s EconiQ gas mixture stands out for its ability to maintain the compact dimensions and reliability of traditional SF6 equipment while significantly reducing environmental impact.

Hitachi Energy is set to revolutionize the high-voltage landscape with the launch of two groundbreaking products at this year’s CIGRE 2024 Paris Session. The first, a fully tested SF6-free 550 kV circuit-breaker, marks a significant leap forward in sustainable high-voltage technology.

Additionally, the company is unveiling the world’s first SF6-free live tank breaker at the 420 kV level, further expanding its portfolio of eco-efficient solutions for the power industry. These innovations demonstrate Hitachi Energy’s commitment to eliminating harmful greenhouse gases while maintaining exceptional performance and reliability.

CIGRE part 2 blog_Guest quotes

Listen to the latest Power Pulse CIGRE special episode part 2 for an in-depth and exciting discussion about the two game-changing EconiQ technologies designed to advance a sustainable energy future.

A sustainable energy future: Hitachi Energy is leading the way

The journey toward a sustainable power grid is complex and demands meticulous planning and innovation. Hitachi Energy’s commitment to developing SF6-free solutions like the EconiQ portfolio is a significant step forward. By addressing both technical and environmental challenges, EconiQ technology not only meets current regulatory requirements but also sets the stage for future advancements in high-voltage product development.

Understanding the high-voltage supply chain is crucial for ensuring the efficiency and reliability of these innovative products. As we move toward a cleaner future, the collaboration between industry leaders, regulatory bodies, and the broader community will be essential in achieving the goal of sustainable power systems.

Hitachi Energy’s dedication to excellence and innovation positions it as a leader in the field, driving the transition to eco-efficient high-voltage products and paving the way for the next generation of power grids.

Connect with our experts to discuss how Hitachi Energy can support your high-voltage needs.


Dr. Markus Heimbach and Dr. Christian Ohler

Dr. Markus Heimbach is an Executive Vice-President and the Managing Director of the High Voltage Products Business Unit at Hitachi Energy.

Markus was a Scientist and Chief Engineer at RWTH Aachen University before joining Hitachi Energy’s predecessor in 1997. He worked in various roles within the Medium Voltage Products Business Unit and led it from 2007 to 2010. From 2010 to 2018, he was the Managing Director of the Transformer Business Unit.

He holds an M.Sc. and a Ph.D. in electrical engineering from RWTH Aachen University, Germany, and an MBA from the University of Hagen, Germany.

Dr. Christian Ohler is the Head of Global Product Group Switchgear of the High Voltage Products Business Unit at Hitachi Energy.

Christian joined the company in 1998 in the Corporate Research Center, Switzerland, and has since gathered extensive experience in research and development, product development, and product and general management. A keen photographer with a curious mind, he firmly believes that it is how people collaborate within the company that makes the difference. 

He holds a Ph.D. in semiconductor physics from RWTH Aachen.