Small footprint, big impact: Decarbonizing the grid one step at a time
Blog Post | 27.11.2024 | 5 min read | Christian Cingolani
Blog Post | 27.11.2024 | 5 min read | Christian Cingolani
Learn about the decarbonization journey and SF₆-free alternatives revolutionizing the future of high-voltage technologies.
Welcome to the Power Pulse podcast blog series, where we delve into the exciting world of energy.
The Power Pulse podcast's new season features the brightest minds in the industry as they examine the challenges, opportunities, innovations, breakthroughs, and sometimes serendipities that have played a part in advancing the development of the power grid. Hear them demystify the fascinating workings behind one of the most impressive engineering feats of the modern era - the electricity grid. Plug in! We promise an electrifying experience with every new episode.
When we think of high-voltage systems, what comes to mind?
If you envisioned sprawling substations, enormous switchgear technologies, and miles and miles of electrical lines stretching across the landscape, you’re exactly right. High-voltage systems encompass many essential (and often large) components, from transmission lines to switchgear. But what if I told you that the future energy grid doesn’t need to occupy as much space – or emit as much carbon? What if high-voltage technologies that are compact in size and low in carbon footprint exist? Well, let me tell you now that it absolutely does!
In this blog, we’ll dive into how minimizing carbon emissions, material use, and spatial footprint is becoming a game-changer when it comes to reshaping high-voltage technologies for a more sustainable energy future.
In the world of energy, the term “footprint” isn’t just about the space it occupies. It’s a double-edged term that involves both carbon footprint and spatial footprint. Both of these factors play a critical role in how sustainable and efficient an energy system can be.
Let’s break down how the footprint of a high-voltage technology impacts the grid.
Carbon footprint refers to the total amount of greenhouse gases emitted into the atmosphere during production, operation, and disposal. In traditional high-voltage systems, like those using sulfur hexafluoride (SF6), the carbon footprint can be quite significant.
While SF6 makes for an excellent insulation gas in switchgear, it is the most potent greenhouse gas. Now more than ever, the industry is on a path to moving away from SF6 and implementing eco-efficient alternatives for a much better and more sustainable grid.
Spatial footprint refers to the physical space a technology requires for its installation and operation. In the past, high-voltage systems like air-insulated substations took up massive amounts of space – covering acres of land. These large systems required significant real estate, which is scarce in an urban environment. Therefore, high-voltage systems that demanded smaller spatial footprints were essential in urban areas and modern energy infrastructure.
In the latest Power Pulse episode, I share expert insights about our EconiQ portfolio and why it’s becoming a real game-changer in decarbonizing the high-voltage grid.
How carbon footprint is measured: Understanding Life Cycle Assessments
Life Cycle Assessment (LCA) is a state-of-the-art method that provides a holistic 360° view of the environmental performance of services and solutions. It quantifies the environmental impact of a product or a system throughout its entire life cycle, providing a clear understanding of critical environmental focus areas for further development.
So, when we talk about a high-voltage product’s carbon footprint, it doesn’t just refer to the insulation gas. The total carbon footprint is based on the following areas that are meticulously evaluated using the LCA approach:
Sustainability has become the central goal and anthem of grids of the future. Over the past decade, the power industry has been integrating renewable energy sources, improving energy efficiency, and implementing SF6-free alternative technologies.
The concept of minimizing footprints is not just a trend; it’s a critical approach to accelerating grid decarbonization. In the energy sector, minimizing both carbon and spatial footprints has a direct impact on reducing overall emissions while enhancing efficiency of power systems. The reduction of carbon emissions from power generation, transmission, and distribution networks is not only an environmental imperative but also an economic opportunity for industries looking to align with global sustainability goals.
One critical aspect of decarbonizing the grid involves transitioning away from SF6-insulated products and upgrading to innovative and eco-efficient technologies such as Hitachi Energy’s EconiQTM.
Below are just a few reasons how EconiQ is revolutionizing the industry:
Big impact 1: Zero-SF6 and lowest carbon footprint
The EconiQ high-voltage portfolio is completely SF6-free, essentially eliminating CO2 equivalent emissions related to the insulation gas. All EconiQ high-voltage products are 100% as reliable and scalable as the conventional solution while delivering the lowest carbon footprint throughout the total life cycle.
Big impact 2: As compact as SF6-based technologies with low material use
The entire EconiQ portfolio retains the size, performance, and reliability of the conventional solution. Its compact design ensures that the technology can be deployed at scale and with speed while minimizing the overall carbon footprint of the grid.
Big impact 3: Reliable and future-proof technology
EconiQ is designed to be future-proof, ensuring compliance with evolving regulatory standards and environmental requirements, therefore providing long-term sustainability in the energy sector.
In the quest for decarbonization, it’s clear that smaller footprints – both in terms of carbon emissions and physical space requirements – hold the key to creating a more sustainable and resilient grid. The beauty of focusing on smaller, smarter SF6-free technologies such as EconiQ lies in the ripple effect they create: less land use, fewer materials, lower emissions, and ultimately, a more flexible and capable grid, able to meet the demands of today’s generation and those to come.
A small footprint today can lead to a big impact for a better tomorrow.
Interested to know more about EconiQ? Visit this page for more information.
Ready to learn more?