Grid-enSure™
Resilience and stability redefined

The new challenges for energy players

The world's energy grids are evolving at an unprecedented pace due to changes in the generation mix, load demand and power eco-system. Without the right actions, the future grid will be more complex, weaker, less controllable, more decentralized,​
and less resilient

Weakness of the grid

The rise in distributed renewable energy sources has decentralized power production. This shift is essential for sustainability but also requires significant adjustments in grid management.

Decentralization of the grid

The decentralization of the grid and the integration of diverse energy sources necessitate sophisticated control systems capable of active demand response.

Lack of resilience and stability of the grid

There is a growing need for technologies providing synthetic inertia, reactive power support, and advanced grid controls to support grid stability.

What is Grid-enSure™?

Grid-enSure™ is a fully integrated portfolio that comprises Hitachi Energy’s top end solutions, present and future, based on Power Electronics and Advanced Control Systems.​ Designed to enhance the flexibility, resilience and stability of the grid

Future-proof solutions available today

The Grid-enSure™ portfolio encompasses cutting-edge Static Compensator (STATCOM), High Voltage Direct Current (HVDC), Static Frequency Converter (SFC) and Energy Storage Solutions (ESS) technologies to deliver future proof functionalities such as fast voltage and frequency support, synthetic inertia, fault current contribution and system strength support. Technology is key for the evolution of the power systems and power electronics based solutions are strategic to enable bulk integration of renewables and utilize the grid to its full potential.

STATCOM

Provides dynamic voltage support and reactive power compensation to enhance grid stability and efficiency.

SFC

Ensures stable frequency conversion for various grid applications, supporting seamless integration of diverse energy sources.

HVDC

Enable high-efficiency, long-distance power transmission, facilitating the integration of renewable energy sources and enhancing grid reliability.

ESS

Digital innovation ecosystem enabling energy management and optimization through battery storage systems, automated and digital capabilities and services.

What’s unique?

The full verticalization of our systems drive value to our customers across: ​
  • Best state-of-the-art functionalities ​
  • Higher reliability thanks to the optimization of the design, material selection and testing ​
  • Ability to meet the demand thanks to the full control on the supply chain
  • Co-creation of new solutions in partnership with our customers
Semiconductors

Semiconductors are the silent heroes in your daily life. They light up homes, power electric cars, drive electric buses, and advance the world’s energy system to be more sustainable, flexible, and secure. Hitachi Energy’s Semiconductors is a motor driven by people, values and innovation to advance a sustainable energy future for all.

 

Power consulting

Hitachi Energy's Power Consulting advisory services holistically assist customers in identifying grid challenges and recommend customized feasible solutions, combining the know-how on the latest technologies including Power Electronics and control systems, with the mastering of standards and local grid codes.

 

Key benefits to redefine grid resilience and stability

Discover how Grid-enSure delivers the essential elements needed to keep your grid resilient, stable and flexible, ensuring reliable power supply and peak performance.

Increasing the reliability of supply

Strengthening the resilience of the grid

Keeping a changing grid under control

Boosting the integration of renewable energy

Increasing power transfer & unlocked capacity

Power Electronics is based on the latest semiconductor technology and allows the fast and secure conversion and control of energy flows

High power density

The latest generation of semiconductors are able to carry +20% more current. The increase in power density translates into higher operational efficiency, reduced footprint, and increased reliability.

+0%

more current

Boosts the integration of renewable energy

Increases power transfer & unlocks capacity

Higher switching frequency

The higher switching frequency of the semiconductors (x10 – x100) reduces the dampening of harmonics into the grid, thus reducing the need of filters in low power applications (i.e. eMobility).

10x-100x higher switching frequency of the semiconductors

Reduces power losses

Increases reliability 
of supply

Our experts' view

Customer Stories

TransnetBW enhanced STATCOM, Germany

The TransnetBW Germany project improves power quality for 11 million people by using innovative SVC Light® STATCOM and a 150 MW storage system, significantly reducing CO2 emissions and enhancing grid stability and efficiency.

Caithness-Moray Shetland 
HVDC Link, UK

The HVDC Links in Scotland project strengthened the power network by integrating renewable energy and linking Shetland to the UK transmission system, using advanced HVDC Light® technology to enhance grid stability and reduce emissions.

+20% current with same size Semiconductor, Worldwide

The new generation of Hitachi Grid-enSure semiconductors offer a 20% increase in current capacity without increasing the size, improving operational efficiency and power density.

Waratah Super Battery, Australia

The new Waratah Super Battery near Sydney will enable the nation’s largest city to keep the lights on, while helping Australia meet its renewable energy target of adding 33,000 gigawatt-hours (GWh) each year through 2030.

We are ready. Are you?

Today we can already face the challenges of the future energy system and make it more sustainable, flexible, reliable and secure.