Hitachi Energy, a global technology leader that is advancing a sustainable energy future for all, today announced that it has been selected by Hydro-Québec for its high-voltage direct current (HVDC) technology for the transmission of electricity, which will ensure the sustainability of the energy exchange between the Quebec network, in eastern Canada, and New York State in the northeastern United States.
Hydro-Québec, the largest hydroelectricity producer in Canada and one of the largest hydroelectricity producers in the world, is a public company that generates, transmits, and distributes reliable, clean and renewable electricity in Québec. Thanks to its surplus energy, it supplies the Canadian provinces and the northeastern United States.
The Châteauguay HVDC system will enable the transmission of up to 1,500 megawatts of electricity between the electrical networks of Quebec and the state of New York which will contribute to maintaining a low carbon footprint in the region. This new system will replace existing equipment which has been in operation since 1984, increasing the efficiency and controllability, plus raising the power conversion capacity of the Châteauguay HVDC system by 50 percent.
“We are proud to be returning to the Chateauguay HVDC station, after helping to build it almost four decades ago,” said Niklas Persson, Managing Director of Hitachi Energy’s Grid Integration business. “This new system represents an important enhancement to the ability to transmit large-scale hydro power between Canada and the United States, which will support the shift away from fossil fuel.”
Hitachi Energy is supplying a “back-to-back” converter station, which converts AC power to DC then reconverts it to AC from DC enabling the interconnection of the 735 kilovolt Canadian and 765 kilovolt New York grids which are “out of phase” and cannot be connected directly via traditional AC systems.
Note to editors:
Hitachi Energy’s HVDC solution combines world-leading expertise in HVDC converter valves; the MACH™ digital control platform, which enables renewables integration and manages voltage and frequency disturbances in the grid; converter power transformers and high-voltage switchgear; as well as system studies, design and engineering, supply, installation supervision and commissioning.
HVDC Light® is a voltage source converter technology developed by Hitachi Energy. It is the preferred technology for many grid applications, including interconnecting countries, integrating renewables and “power-from-shore” connections to offshore production facilities. HVDC Light’s defining features include uniquely compact converter stations and exceptionally low electrical losses.
Hitachi Energy pioneered commercial HVDC technology almost 70 years ago and has delivered more than half of the world’s HVDC projects.