Transformers for railway

The fast urbanization, the increasing demand for mobility, and the excess of CO2 emissions are developing fast. It has never been so important to provide efficient and reliable transportation solutions consuming less energy and delivering more uptime at the lowest cost of ownership. Our purpose is to help our customers to meet their mobility demands on rail, land, water, and air, without consuming the earth.

Safer, greener, consuming less.
 

The future of Transport: towards a carbon-neutral vision

The global demand for transport is growing fast wherein, based on given present trends, passenger and freight transportation activities will be more than double by 2050. This growth carries with it greater energy demand, increased in carbon dioxide (CO2) emissions, and atmospheric pollutants. Rail travel has been well-matched to a world that is becoming more urbanized. 

With rail being among the most energy-efficient mode of transport for freight and passengers, the heavy reliance on electricity makes the rail sector the most energy-diverse mode of transport.

Together with Hitachi Energy and anchored by our mission, the purpose of helping our customers meet their mobility demand with green, safe, reliable, and efficient railways with low operating costs. This is how we will achieve a sustainable energy transition - globally.

 

Source of rail data: IEA - The Future of Rail

75%

of passenger rail transport is electrified

50%

of freight rail transport is electrified

Electrification is enabling rail mobility

Why Hitachi Energy for railways

Worldwide leader
Global component supplier to most of the world’s rail and metro system integrators, EPCs, and power network operators
Revenues
> 100 MUSD/year in rail infrastructure transformers globally
 
16 factories
Global footprint for manufacturing liquid-filled and dry-type transformers for rail infrastructures
 
Complete portfolio
The broadest portfolio of dry and liquid transformers to support more than 15 product applications
> 5,000 units in operations 
The largest installed base of rail infrastructure transformers in operation worldwide

Our Railway Portfolio

​Rail infrastructure transformers, or railway transformers, are used in the rail and metro network systems for many reasons: they reduce the voltage from an HV power network to a suitable level to feed the AC railway catenary conductors at 50 or 60 Hz, they collect the return current from the rails to the return conductor of the rail network system, they are used to feed converter stations to supply power to DC lines or lines at 16.7 or 25 Hz, they are used to feed auxiliary networks (for lighting purposes, for heating the wagons when the train is steady, or for heating or powering some critical railway points), and they can be used as insulation transformers to isolate the AC network from the DC leakage currents caused by DC rails when in close proximity of AC rails.

Transformadores de reforço
Transformadores de reforço da Hitachi Energy são usados em alimentadores catenários CA ferroviários elétricos para coletar a corrente de retorno dos trilhos e do terra para o condutor de retorno. Clique para saber mais.
AC Line Feeder Autotransformers
AC Line Feeder Non-​​Autotransformer
Learn more
Learn more
Auxiliary transformers
Hitachi Energy designed compact Auxiliary transformers for lighting, heating the train wagons, or producing single-phase auxiliary for safety supply. Click to learn more.
Transformadores de isolamento
Os transformadores de isolamento são transformadores especiais que isolam a rede CA das correntes de fuga CC causadas por trilhos CC nas proximidades dos trilhos CA. Clique para saber mais.
Part of categoryPress Release
innovative oil-free and plug-and-play traction transformers
Hitachi Energy launches innovative oil-free and plug-and-play traction transformer
Hitachi Energy announced the launch of its innovative oil-free traction transformer RESIBLOC® Rail, with integrated cooling system at InnoTrans at the Berlin.
21-09-2022 | 3 min read
Part of categoryCustomer Story
Scott Transformers to strengthen the Indian Railways power system
Strengthening the power supply system in railways

Contact us

Submit your enquiry and we will contact you