Hitachi Energy will provide onshore and offshore grid connection equipment and power quality solutions to ScottishPower Renewables, part of the Iberdrola Group, a global leader in renewable energies. The project will enable the integration of 960-megawatt (MW) of renewable electricity from the East Anglia TWO (EA TWO) wind farm, located 32 km off the Suffolk coast of England. This will provide enough green power for the equivalent of almost one million homes and significantly contribute to the UK's 2030 energy targets.
The energy landscape is growing at an unprecedented pace, and integrating renewables into the grid at scale reveals new challenges, such as lack of inertia, power imbalances, limited interconnections, and voltage instability. Through projects like EA TWO, Hitachi Energy's domain expertise and large installed base in power quality solutions are helping countries overcome these challenges to enhance the use of renewable energy and meet carbon neutrality targets.
In this spirit of collaboration and co-creation, Hitachi Energy and ScottishPower Renewables have set new advanced solutions and quality standards to accelerate the energy transition through offshore wind.