Choisissez votre région et votre langue

Menu

General Information:

Hitachi Energy is a world leader in the area of Power Quality Solutions (PQS). Hitachi Energy was the first to introduce Flexible AC Transmission System (FACTS) technology to the power industry and has delivered solutions for the more than 50 years now. Hitachi Energy has a number of solutions that enhance the security, capacity and flexibility of power transmission systems. These solutions enable power grid owners to increase existing transmission network capacity while maintaining or improving the operating margins necessary for grid stability.  Hitachi Energy has the full FACTS portfolio and in-house manufacturing of key components.

Hitachi Energy uses a very high-end system for its control, protection and monitoring. This system is called as MACH. This computerized system is built with the state-of-the-art electronics, microprocessors and digital signal processors, connected by high performance industry standard busses and fiber optic communication links. They operate on very high standard application software designed by the control design team for which there is a need for experienced control system engineers.

Your Responsibilities:

  • Design, implementation, verification, and commissioning of the MACH control system to meet our customer’s requirements.
  • Responsible for design, time schedule, budget, and quality of deliverables during the entire project execution process for control scope
  • Developing control algorithms/ firmware and modeling/simulation for power converters/ control development
  • Extensive contact with other engineering groups, the project manager, local Hitachi offices and externally to our customer during factory acceptance and commissioning phase.
  • Ability to travel to sites to support commissioning of MACH control system
  • Stay current with the latest technology and always open to learn new developments
  • Legally authorized to work in the United States
  • Living Hitachi Energy's core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Your Background:

  • Create, modify, debug, test and deploy control algorithms
  • Candidate must already have work authorization that would permit them to work for Hitachi Energy in the United States.
  • Control logic design and testing
  • Hardware-in-the-Loop (HIL) testing with real-time simulators
  • Prepare customer submittals and test procedures
  • Factory acceptance test, customer meetings, technical support
  • Ready for travel to sites to support commissioning of MACH system and test records documentation
  • Qualification & Experience:
  • M.Sc./Ph.D. Power Systems / Power Electronics/ Control Theory
  • Candidate should have 5+ years’ experience in Design and testing of PI/PID or similar control algorithms
  • Specific Knowledge & Skillsets:
  • Strong understanding on FACTS applications
  • Deep knowledge on control theory and power electronics applications
  • Design and testing of PI/PID or similar control algorithms
  • Experience in simulation using MATLAB or real time simulators
  • Good knowledge on power system - signal processing, active and reactive power concepts will be an added advantage
  • Knowledge on VHDL and DSP basics will be an added advantage.
  • Soft skills:
  • Individual contributor using in-depth knowledge in a specific area to execute complex or specialized projects / challenges often thinking independently to challenge traditional solutions.
  • Comprehensive knowledge of related disciplines in the organization.
  • Works independently, applying established standards
  • Good communication skills
  • Dynamic and Proactive, willing to grow in the organization
  • Team player, ready to play the role across the different countries
  • High level of ownership

Lieu Raleigh, North Carolina, United States of America
Type d'emploi Full time
De l'expérience Experienced
Fonction du poste Engineering & Science
Contrat Regular
Date de publication 2024-10-04
Numéro de réference R0063115

À propos de Hitachi Énergie

Hitachi Énergie est un chef de file technologique mondial voué à la promotion d’un avenir énergétique durable pour tous. Nous servons des clients dans les secteurs des services publics, de l'industrie et des infrastructures avec des solutions et des services innovants tout au long de la chaîne de valeur. Avec nos clients et nos partenaires, nous sommes pionniers en matière de technologies et permettons la transformation numérique nécessaire pour accélérer la transition énergétique vers un avenir carboneutre. Nous faisons progresser le système énergétique mondial pour qu'il devienne plus durable, plus flexible et plus sûr, tout en équilibrant les valeurs sociales, environnementales et économiques. Hitachi Énergie est forte d’une expérience avérée et dispose d’une base installée inégalée dans plus de 140 pays, Avec son siège social établi en Suisse, la société emploie plus de 45 000 personnes dans 90 pays et génère des volumes d’affaires de plus de 13 milliards de dollars US.
www.hitachienergy.com

Hitachi Energie est un employeur qui prône l'égalité des chances en matière d'emploi et l'action positive, et qui encourage la diversité sur le lieu de travail. Nous vous invitons à poser votre candidature et tenons à ce que vous sachiez que tous les candidats qualifiés seront pris en considération pour un emploi sans distinction de race, de croyance, de couleur, d'ascendance, de religion, de sexe, d'origine nationale, de statut de citoyen, d'âge, d'orientation sexuelle, d'identité de genre, de handicap, d'état civil, de statut de congé médical familial, de statut d'ancien combattant protégé ou de toute autre caractéristique protégée par la loi. Pour plus d'informations sur vos droits en matière d'égalité des chances en tant que candidat, veuillez consulter le site web suivant : ici. Les personnes qualifiées souffrant d'un handicap peuvent demander un aménagement raisonnable si leur handicap les empêche d'utiliser le site de carrière de Hitachi Énergie ou les limite dans leur capacité à y accéder. Vous pouvez demander des aménagements raisonnables en appelant un représentant des ressources humaines de Hitachi Énergie au 1-888-504-2007 ou en envoyant un courriel à : [email protected]. Notez que les CV et les candidatures envoyés à ces coordonnées ne seront pas acceptés.