Choisissez votre région et votre langue

Menu

Field Service Technician A

General information:

Hitachi Energy is seeking a Transformer Field Supervisor & Tester for its South Boston, VA location. This role is responsible for directing and working alongside crews of field service technicians as they complete various transformer installation, repair, maintenance, and inspection projects. Transformer Service Testers have the technical knowledge and ability to perform standard electrical testing on these transformers. Work is performed on customer sites and requires extensive travel. This position reports into the Eastern U.S. region but projects may be assigned anywhere in the United States.

Responsibilities:

Lead crews ranging from 2 to 8+ technicians to complete assigned projects Projects may include but are not limited to the installation, repair, testing, maintenance, relocation, scrap, inspection, and retrofit of transformers with high-side voltages ranging from 4160V to 765kV Act as the onsite point of contact for the customer and subcontractors during project execution Strategically assign tasks to crew members in order to minimize cost and project duration considering crew skillsets, site conditions, weather forecasts, etc. Proactively identify and report project nonconformance to Project Management and Engineering for timely resolution Perform electrical testing of transformers and reactors including but not limited to bushing power factor & capacitance, core megger, CT ratio & polarity, TTR, winding resistance, insulation power factor, insulation resistance, excitation, SFRA, DRF, leakage reactance, and control cabinet functional checks Provide input and expertise during the project-planning phase regarding project schedule and manpower requirements Practice and promote a safety-first approach; always maintain compliance with all Hitachi Energy and customer EHS requirements

Your background:

High School Diploma/GED and a minimum 9 years of professional work experience, or Associate Degree and a minimum 7 years of professional work experience. Candidates must already have a work authorization that would permit them to work for Hitachi Energy in the US. Thorough knowledge of transformer field service operations and transformer field testing Knowledgeable and fully fluent in transformer installation and assembly, vacuum and oil processing, shell and/or core form transformer designs, and components internal to the transformer Proficiency with Load Tap Changer (LTC) maintenance and repair is a plus Experience welding above and below oil on transformer tanks is a plus Possession of a Class A CDL is a plus Must have a valid driver's license and ability to travel 90%

Lieu South Boston, Virginia, United States of America
Type d'emploi Full time
De l'expérience Experienced
Fonction du poste Engineering & Science
Contrat Regular
Date de publication 2023-08-21
Numéro de réference R0026833

À propos de Hitachi Énergie

Hitachi Énergie est un chef de file technologique mondial voué à la promotion d’un avenir énergétique durable pour tous. Nous servons des clients dans les secteurs des services publics, de l'industrie et des infrastructures avec des solutions et des services innovants tout au long de la chaîne de valeur. Avec nos clients et nos partenaires, nous sommes pionniers en matière de technologies et permettons la transformation numérique nécessaire pour accélérer la transition énergétique vers un avenir carboneutre. Nous faisons progresser le système énergétique mondial pour qu'il devienne plus durable, plus flexible et plus sûr, tout en équilibrant les valeurs sociales, environnementales et économiques. Hitachi Énergie est forte d’une expérience avérée et dispose d’une base installée inégalée dans plus de 140 pays, Avec son siège social établi en Suisse, la société emploie plus de 45 000 personnes dans 90 pays et génère des volumes d’affaires de plus de 13 milliards de dollars US.
www.hitachienergy.com

Hitachi Energie est un employeur qui prône l'égalité des chances en matière d'emploi et l'action positive, et qui encourage la diversité sur le lieu de travail. Nous vous invitons à poser votre candidature et tenons à ce que vous sachiez que tous les candidats qualifiés seront pris en considération pour un emploi sans distinction de race, de croyance, de couleur, d'ascendance, de religion, de sexe, d'origine nationale, de statut de citoyen, d'âge, d'orientation sexuelle, d'identité de genre, de handicap, d'état civil, de statut de congé médical familial, de statut d'ancien combattant protégé ou de toute autre caractéristique protégée par la loi. Pour plus d'informations sur vos droits en matière d'égalité des chances en tant que candidat, veuillez consulter le site web suivant : ici. Les personnes qualifiées souffrant d'un handicap peuvent demander un aménagement raisonnable si leur handicap les empêche d'utiliser le site de carrière de Hitachi Énergie ou les limite dans leur capacité à y accéder. Vous pouvez demander des aménagements raisonnables en appelant un représentant des ressources humaines de Hitachi Énergie au 1-888-504-2007 ou en envoyant un courriel à : [email protected]. Notez que les CV et les candidatures envoyés à ces coordonnées ne seront pas acceptés.