Selecciona tu región e idioma

Menú

Press Release Santiago de Chile, Chile 09-11-2023

3 min read

Mobile grid connection helps Chilean copper mine grow

A Grid-eXpand™ Mobile digital grid connection will help the copper mine extend production to new and deeper areas of the site, allowing the mine operator to quickly deploy the grid connection where needed.

Copper demand is expected to double by mid-century as the transition to a sustainable, digitized electricity-based energy system intensifies. Copper is used in most electronic and electrical products, and is a key component in electric vehicles, wind turbines, solar panels and power grids. It is also recyclable.

About 25% of the world's copper is mined in Chile. As production extends to new or deeper parts of the site, access to a constant flow of electricity is needed to power mining equipment and facilities.

To expand and strengthen the energy system, the mining company awarded the EPC company Sigdo Koppers Engineering and Construction (SKIC) the Engineering (through its subsidiary company Dessau), Procurement and Construction of this important project, which allows the mining company to relate to a single representative and responsible party.

SKIC has relevant experience in power transmission lines, both in Chile and Brazil (more than 7,000km installed in total), and in this opportunity, the participation of Hitachi Energy in the execution of this contract stands out.

To provide this electricity SKIC chose Hitachi Energy's mobile digital grid connection that can be easily moved from one location to another as the needs may dictate. Hitachi Energy has been supplying mobile grid connections for more than 40 years. It offers the highest power (500 MVA), the highest voltage (420 kV), the smallest footprint and the best maneuverability in the market.

Grid-eXpand Mobile solutions are modular, prefabricated, pre-assembled and pre-tested for fast delivery and plug-and-play implementation. They are easy to transport fully assembled and comply with all road transport regulations (length, height, and width), which means they are easy to deploy and can reach even the least accessible locations, including mountainous desert terrain. Once on site, they take only hours to install and energize.

For this application, Sigdo Koppers Ingeniería y Construcción chose a 69/13.8 kV grid connection, which connects to the mine's power grid. The solution is housed in modules on two trailers, with high voltage equipment on one trailer and medium voltage, auxiliary and control and protection equipment on the other.

Impact

Hitachi Energy to design, deliver and commission mobile grid connection by February 2024 to help increase the capacity and reach of the mine's power grid.

The solution will provide the mine with maximum deployment flexibility, allowing it to quickly move the grid connection to wherever it is needed. Digitally enabled, the network connection will transmit real-time data to the control center for fast, informed data entry, analysis, and decision-making.

The solution builds on Hitachi Energy's installed base of more than 400 mobile grid connections delivered to utilities, transmission system operators and industries worldwide.

Hitachi Energy will also design and deliver a permanent gas-insulated grid connection, which will connect to the national transmission grid to expand the mine's power capacity.

About Hitachi Energy

Hitachi Energy is a global technology leader that is advancing a sustainable energy future for all. We serve customers in the utility, industry and infrastructure sectors with innovative solutions and services across the value chain. Together with customers and partners, we pioneer technologies and enable the digital transformation required to accelerate the energy transition towards a carbon-neutral future. We are advancing the world's energy system to become more sustainable, flexible and secure whilst balancing social, environmental and economic value. Hitachi Energy has a proven track record and unparalleled installed base in more than 140 countries. We integrate more than 150 GW of HVDC links into the power system, helping our customers enable more wind and solar. Headquartered in Switzerland, we employ more than 40,000 people in 90 countries and generate business volumes of over $10 billion USD. 

https://www.hitachienergy.com

https://www.linkedin.com/company/hitachienergy

https://twitter.com/HitachiEnergy

About Hitachi, Ltd.

Hitachi drives Social Innovation Business, creating a sustainable society through the use of data and technology. We solve customers' and society's challenges with Lumada solutions leveraging IT, OT (Operational Technology) and products. Hitachi operates under the 3 business sectors of “Digital Systems & Services” – supporting our customers’ digital transformation; “Green Energy & Mobility” – contributing to a decarbonized society through energy and railway systems, and “Connective Industries” – connecting products through digital technology to provide solutions in various industries. Driven by Digital, Green, and Innovation, we aim for growth through co-creation with our customers. The company’s revenues as 3 sectors for fiscal year 2023 (ended March 31, 2024) totaled 8,564.3 billion yen, with 573 consolidated subsidiaries and approximately 270,000 employees worldwide. For more information on Hitachi, please visit the company's website at https://www.hitachi.com.

Contacts

Angelica Concha
Angelica Concha

Country Communications Manager | Chile