Press Release Bangalore, India 09-03-2021

2 min read

Hitachi ABB Power Grids wins INR 160 crore order to supply transformers to Indian Railways

beautiful morning image of two Indian train with rail between them in yellowish morning light and a bit fogg. Perfect to show Indian railways system in news or article

The global technology leader will support India’s mission to make Indian Railways a net-zero carbon emitter by 2030

Bangalore, March 10 2021 – Hitachi ABB Power Grids in India (listed on the stock exchanges as “ABB Power Products and Systems India Limited”) has won orders worth INR 160 crore from the Government of India’s electric locomotive manufacturer, Chittaranjan Locomotive Works (CLW), and the Central Organization for Rail Electrification (CORE), to power electric freight locomotives for the Indian Railways.

For CLW, Hitachi ABB Power Grids will deliver traction transformers for one of Indian Railways’ most successful class of locomotives, the WAG 9, which was developed in response to strong growth in the rail freight transportation sector; for CORE, it will supply trackside transformers.

Indian Railways manages the fourth-largest rail network in the world by size. It is aiming to create a future-ready railway system, bringing down logistics costs for industry and supporting the Make-in-India initiative. This plan aligns with the government’s goal of achieving 100 percent rail electrification by December 2023 and making Indian Railways a net-zero carbon emitter by 2030.

“These orders are a source of immense pride for us at Hitachi ABB Power Grids. They advance our vision of playing a pivotal role in rail electrification in India and enabling improvements in rail safety, capacity and speed,” said N Venu, CEO and Managing Director, Hitachi ABB Power Grids in India. “Such partnerships will help lower our dependence on imported fossil fuel and reduce both fuel costs and carbon emissions for the Indian Railways,” he added.

Hitachi ABB Power Grids will deliver trackside transformers rated 132 kV (kilovolt) to CORE and traction transformers rated 25 kV to CLW. The trackside transformers reduce power voltage from the utility power network to a suitable level before feeding it to the railway catenary conductors. Traction transformers route power from the catenary  for essential train functions such as traction, lighting, ventilation, braking, signaling and communication. 

About Hitachi Energy

 

Hitachi Energy is a global technology leader that is advancing a sustainable energy future for all. We serve customers in the utility, industry and infrastructure sectors with innovative solutions and services across the value chain. Together with customers and partners, we pioneer technologies and enable the digital transformation required to accelerate the energy transition towards a carbon-neutral future. We are advancing the world’s energy system to become more sustainable, flexible and secure whilst balancing social, environmental and economic value. Hitachi Energy has a proven track record and unparalleled installed base in more than 140 countries. Headquartered in Switzerland, we employ around 38,000 people in 90 countries and generate business volumes of approximately $10 billion USD.

Contacts

Photo of
Manashwi Banerjee

Head of Communications - India and South East Asia

Hitachi Energy

Todas las noticias