Customer Story


Caithness Moray Shetland
The first multi-terminal HVDC VSC interconnection in Europe

Challenge

Project Details


Customer: 
 Scottish and Southern Electricity Networks (SSEN) Transmission​

Location: Scotland, UK

Scope: Three HVDC Light® converter stations​ in multi-terminal scheme, executed in two stages:

  • Caithness-Moray link commissioned in 2018 and prepared for further expansion
  • Shetland link operating since Aug ‘24

Client’s needs: To connect the Shetland to the UK transmission system whilst strengthening onshore network in Northern Scotland

Solution

Three HVDC Light® converter stations connected in multi-terminal scheme Based on Hitachi Energy HVDC Light® VSC technology
 Symmetric monopole ±320 kV DC
​Blackhillock (1,200 MW) – stabilizes the DC grid through DC voltage control
​Kergord (600 MW) – stabilizes Viking wind farm on Shetland through frequency and AC voltage control
​Multi-purpose HVDC for up to five converter stations and two solutions for multi-terminal connection point
Spittal (800 MW) – stabilizes Caithness AC network through grid forming control
DC Grid Master Controller to coordinate all signals and sequences, already implemented at first stage
Detail multi-terminal studies for up to 5 stations. Off-line simulation studies using Virtual Control & Protection (vMACH) for efficiency and early risk mitigation

Impact

Multi-terminal HVDC interconnection provides flexibility to transfer power in multiple directions,​ based on supply and demand, with minimal power losses
Contribute to bringing all greenhouse gas emissions to net zero by 2050
Enhance grid performance and resilience through voltage and frequency control​
​Help to connect and transmit wind power generated on the islands to the UK
A future proof solution boosting the integration of renewable energy ​

Return to the Grid-enSure™ page to explore our innovative portfolio and discover more success stories showcasing the powerful impact of our solutions.